Technical FAQs

Ask a Question

What fuse is required for the Conext CL?



For calculating the PV fuse rating for a specific PV array installation, refer the PV panel manufacturer documentation in addition to local electrical installation code.

Recommended Fuse: Part number: PV1510F

Make: Cooper Bussman

Rating:1000 VDC, 15 A.

Note: Not applicable for Base model.

Was this helpful?
What can we do to improve the information ?