Technical FAQs

Ask a Question

What is the maximum wire size the XW MPPT60 can accommoodate?

  The MPPT60 is not approved for use with conductors larger than #6AWG, however it
is possible to use an external splice block that allows for larger conductors to be used. This is outlined on pg.2-16 of the attached manual. 
Was this helpful?
What can we do to improve the information ?