Technical FAQs

Ask a Question

My Conext CL shows event 4700 Low power fault. What does this mean?

Event 4700 Low Power Fault indicates that there is not enough power available from the PV array to bring the inverter online.  Once the power available from the array increases, the event will clear and the inverter will begin production.  Possible causes of low power production by the PV array are:

1) Low Solar irradiance in the early morning or late evening
2) High cloud cover reducing solar irradiance
3) Excessive shading of the PV array
4) A defective PV module or wiring in the array
Was this helpful?
What can we do to improve the information ?