Technical FAQs

Ask a Question

Are the solar ATV312 drives sold in the USA?

Issue:
Are the solar ATV312 drives sold in the USA?

Product Line:
Altivar ATV312 Solar only

Environment:
Only the Solar version of the ATV312

Cause:
Would like to order a Solar version ATV312 drive

Resolution:
Per Product Marketing they are not available for sale in the USA.  If a customer is interested in purchasing, they need to work with the Local Sales office to determine the number of units needed per month and the Local Sales office will contact the Marketing Department. 
(udpated July 2015).
 
Was this helpful?
What can we do to improve the information ?