Technical FAQs

Ask a Question

Will the 120V adaptor card (VW3A3101) work with an I/O extension or Communication card installed on the drive?

Issue:
Will the 120V adaptor card (VW3A3101) work with an I/O extension or Communication card installed on the drive?

Product Line:
ATV61/71, VW3A3101, VW3A3201 and VW3A3201

Environment:
All serial numbers for ATV61/71, VW3A3101, VW3A3201 and VW3A3201

Cause:
N/A

Resolution:
Yes the 120 Vac adaptor card will work with that I/O extension card or any other option card.
The adaptor card (VW3A3101) plugs into the main terminal card of the drive.
The option cards are attached underneath the top cover of the drive. Only a maximum 2 can be attached at a time.

 
Was this helpful?
What can we do to improve the information ?