Technical FAQs

Ask a Question

Is the motor service factor a programmable option in the Tesys T Motor Controller?

Product line:
Tesys T Motor Controllers

Resolution:
Service factor is not a changable option within the Tesys T programming. The Tesys T will automatically take into account a standard service factor of 1.15-1.25, outside of this standard service factor range a multiplier should be applied to the full load current that is programmed in the Tesys T. This multiplier can usually be provided by the motor manufacturer.

Was this helpful?
What can we do to improve the information ?