Technical FAQs

Ask a Question

What is the BACnet Unit Load for ATV212?

Issue:
What is the BACnet Unit Load for ATV212?

Product Line:
ATV212, Altivar 212

Environment:
All

Cause:
Customer is designing BACnet Network

Resolution:
The unit Load is 32. According to the TIA-485A standard, a single unit load is equivalent to a 12 kohm impedance attached to the + and – data lines (connected to ground or supply).
Was this helpful?
What can we do to improve the information ?