Technical FAQs

Ask a Question

What color is the HOM120DF and HOM115DF test button?

Issue:
What color are the HOM and QO "Dual-Function" breaker test buttons (such as HOM120DF and HOM115DF)?

Product Line:
QO and Homeline Dual-Function breakers

Environment:
48840-248-01  QO and QOB combination arc fault breaker instructions that come with the breaker, includes the CAFI Fault Indication Procedure
48840-249-01  HOM combination arc fault breaker instructions that come with the breaker, includes the CAFI Fault Indication Procedure
HRB86114  Dual Function HOM instructions
HRB73152  Dual Function QO instructions

Resolution:
The test buttons for the QO-DF or HOM-DF dual function breakers are purple. 
NOTE:  QO and Homeline dual function breakers have both arc fault and GFI protection.
NOTE:  AFI breakers have blue or green test buttons; CAFI breakers have white test buttons.
Was this helpful?
What can we do to improve the information ?