Technical FAQs

Ask a Question

What are the repair parts for the CHU364DS, Series F6 (may be shown as F06)?

Issue:
Current Design Repair parts

Product Line:
Heavy Duty Safety Switches

Environment:
Repair Parts

Cause:
Maintenance

Resolution:
The repair parts for the CHU364DS, series F6 (F06) are as follows. No other parts are available.

Complete Line/Load Base (all one piece) - 4056704050 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line Base mounting screws - 4020546401 (requires 6 per line base)
Arc Suppressor Assembly - 4056677550 (requires one per phase or pole)
Arc Suppressor mounting screw - 4020514501 (requires one per Arc Suppressor)
Lug Assembly - CL20F (incl. 6 lugs - requires mounting screws below)
Lug Assembly mounting screw - 2140122240 (per lug)
Switch Mechanism - 4056678650 (also requires mechanism coupling assembly 4056699850 and interlock connector assembly 4056718850)
Switch Mechanism mounting screws- 2299940562 (requires 2)
Handle Assembly - 4056736850
Lockplate - 4056738901
Lockplate mounting screws - 2194900001 (requires 2)
Was this helpful?
What can we do to improve the information ?