Technical FAQs

Ask a Question

Can the Conext Monitor 20 show data from period prior to monitor installation?

Application: Monitor Conext RL and Conext TL Solar inverters.
Can the Conext Monitor 20 pull historical logs from the inverter prior to the monitor being installed in the system?


Answer:The Conext Monitor 20 cannot pull historical logs, it only takes data when in operation and can not get data prior to the Conext Monitor being installed.
 
Was this helpful?
What can we do to improve the information ?