Technical FAQs

Ask a Question

Is the Y47 Form for an extra cover gasket available for the 8536 Type S starters?

Issue:
I want to use the Y47 Form on my 8536 Type S starter.

Product Line:
8536 Type S Starters

Environment:
US Product Lines

Cause:
The product selector will not let me select that option, but it shows it in the Digest as an option.

Resolution:
The Y47 Form for an extra cover gasket is not available for the 8536 Type S starters. It is only available for the Class 8538, and 8539 combination starters.
 
Was this helpful?
What can we do to improve the information ?