Technical FAQs

Ask a Question

I purchased a C60 but the circuit board says C40

The C60 uses the C40 circuit board, however certain components are rated for a higher DC voltage because C40 can be set for 48V.
The fact that the 48V jumper position is missing confirms a C60. 
Was this helpful?
What can we do to improve the information ?