Technical FAQs

Ask a Question

Can I program the ATV61 HMI fwd/rev button, independent of local start/stop buttons?

Issue:  
Can I program only the fwd/rev button with start/stop in remote mode?  
 
Product Line:
ATV61, ATV71

 Environment:
 All
 
 Cause:
Maintenance configuration request.
 
Resolution:
No, fwd/rev on the HMI can not be programmed independent of local start/stop commands 
Was this helpful?
What can we do to improve the information ?