Technical FAQs

Ask a Question

What is the operational limitation of the frequency of the voltage in an LC1D contactor?

Issue:
What is the operational limitation of the frequency of the voltage in an LC1D contactor?

Product Line:
TeSys D Contactors - GIC Product

Environment:
US Product

Cause:
Some industries use these contactors at Hertz frequencies besides 50/60hz

Resolution:
The LC1D contactors have the limitation of 25-400hz.  The specifications are attached.
Was this helpful?
What can we do to improve the information ?