Technical FAQs

Ask a Question

What are the replacement coils for 8903SP lighting contactors?

Issue:
What are the replacement coils for 8903SP lighting contactors?

Product Line:
8903 NEMA Lighting Contactors - GIC Product

Environment:
US Product

Cause:
Replacement parts - Product Characteristics

Resolution:
The following coils are available:
2-3 Pole Versions:
     31063-409-16 - 24Vac
     31063-409-42 - 120Vac
     31063-409-44 - 208Vac
     31063-409-47 - 240Vac
     31063-409-49 - 277Vac
     31063-409-57 - 480Vac
     31063-409-60 - 600Vac
4-5 Pole Versions:
     31063-400-16 - 24Vac
     31063-400-42 - 120Vac
     31063-400-44 - 208Vac
     31063-400-47 - 240Vac
     31063-400-49 - 277Vac
     31063-400-57 - 480Vac
     31063-400-60 - 600Vac
 
Was this helpful?
What can we do to improve the information ?