Technical FAQs

Ask a Question

Can the VW3A31101 ATV312 HMI be configured to toggle from local to remote mode?

Issue:
Can the VW3A31101  ATV312 HMI be configured to toggle from local to remote mode?
 
Product Line:
ATV312
 
Environment:
All
 
Cause:
Need to toggle modes from HMI
 
Resolution:
 
No, that configuration is not available with VW3A31101 .
Was this helpful?
What can we do to improve the information ?