Technical FAQs

Ask a Question

Is Conext Battery Monitor compatible with XW4024 legacy model?

The XW4024 (865-1010) was discontinued before release of XW+NA models. Newer firmware was never developed 
for the XW4024 so it would be compatible with the Conext Battery Monitor (i.e. Start SOC%), which can still be used
as a stand-alone battery monitor viewable in SCP that does have the latest firmware.
Was this helpful?
What can we do to improve the information ?