Technical FAQs

Ask a Question

How many analog output are available on the Altivar 312 drives?

Issue:
How many analog output are availables on the Altivar 312 drives? 
 
Product Line:
ATV312

Evironment:
All

Cause:
Application requires 2 analog outputs

Resolution:
Only one analog output per drive. No previsions or options for additional input or outputs. 





 
Was this helpful?
What can we do to improve the information ?