Technical FAQs

Ask a Question

Conext XW+ shows fault F52 EEPROM Error.

Unit displays F52 EEPROM Error

Solution:Power cycle the unit and leave it off until voltage falls below<2 volt on terminals of the inverter(Wait about 20-30 min)
Re power the unit, if fault still persists then the next step is to perform a restore to default
If the fault still ocurrs after power cycle and restore to defaults unit needs to be replaced
Was this helpful?
What can we do to improve the information ?