Technical FAQs

Ask a Question

What is the difference between 9065SF and 9065ST MotorLogic Overload units size 2-4?

Issue:
What is the difference between 9065SF and 9065ST MotorLogic Overload units size 2-4?

Product Line:
NEMA Starter Accessories - GIC Product

Environment:
US Product

Cause:
Product Characteristics

Resolution:
The 9065ST units are designed to be replacement units and have bubars built into them to facilitate direct mounting.
Was this helpful?
What can we do to improve the information ?