Technical FAQs

Ask a Question

Are Compact NSJ breakers 100% rated?

Issue:
Are Compact NSJ breakers 100% rated?

Product Line:
Compact NSJ

Environment:
UL Listed Breakers sold in USA

Resolution:
All NSJ breakers are 100% rated EXCEPT those with 600A sensors and 400A 4p with OSN (Over-Sized Neutral).
Otherwise stated:
All NSJ250 and NSJ400 3p breakers are 100% rated.  600A and 400A with OSN are only available as 80%.
Was this helpful?
What can we do to improve the information ?