Technical FAQs

Ask a Question

What is Conext SW THD% spec?

Even though this specification is not published in product literature, the THD is less than 5% with the normal input voltage range 44V-56V.
When the input voltage range is 40V-44V, the THD is less than 8%. The tests are conducted under pure resistive load condition.
Was this helpful?
What can we do to improve the information ?