Technical FAQs

Ask a Question

What is the lug wire range on a 82345 or 82345R?

Issue:
Application

Product Line:
DT Switch

Environment:
Application

Cause:
Clarify feature

Resolution:
The lugs will accept (1) #1/0 - 600 kcmil or (2) #1/0 - 300 kcmil. There are no optional lugs available.
Was this helpful?
What can we do to improve the information ?