Technical FAQs

Ask a Question

How do you disable the stop button on the remote VW3A1101 ATV61 or ATV71 HMI?

Issue:
How do you disable the stop button on the remote VW3A1101 ATV61 or ATV71 HMI?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Wants to disable the stop button on the remote HMI.

Resolution:
Warning Warning:  If you disable the stop button on the HMI the drive will not stop if you push the stop button.  If you disable this you will assume all liability.  We do not recommend that you disable the stop button on the drive.

Programming
Drives menu  then
menu 1.6 Command menu
Stop key priority  set to No.
Was this helpful?
What can we do to improve the information ?