Technical FAQs

Ask a Question

Why does SoMove not show phase B current on an ATS22 with the Q suffix in the monitor menu?

Issue:
SoMove monitor input current
 
Product Line:
ATS22
 
Environment:
Q suffix
 
Cause:
None
 
Resolution:
The "Q" versions are european model and these do no have current transformers on phase "B".  Therefore the monitor in SoMove will not show this phase.
 
Was this helpful?
What can we do to improve the information ?