Technical FAQs

Ask a Question

Is there a NEMA 1 enclosure for Size 3 and larger starter with space for a control transformer?

Issue:
Is there a NEMA 1 enclosure for Size 3 and larger starter with space for a control transformer?

Product Line:
NEMA Starters - GIC Product

Environment:
US Product

Cause:
Product Characteristics and Identification

Resolution:
The standard size enclosures will not have room for a transformer, and oversize enclosures are not available for a size 3 or larger.  The entire starter must be ordered with transformer and enclosure specified as part of the starter in the product selector tool.
 
Was this helpful?
What can we do to improve the information ?