Technical FAQs

Ask a Question

What is the part number for the standard terminal block which includes the auxiliary contacts and the coil terminals on the LUB12/32?

Issue:
What is the part number for the standard terminal block which includes the auxiliary contacts and the coil terminals on the LUB12/32?

Product Line:
U-Line Starters - GIC Product

Environment:
US Product

Cause:
Product Selection

Resolution:
The terminal block is part is LU9BN11
 
Was this helpful?
What can we do to improve the information ?