Technical FAQs

Ask a Question

How do I know what the voltage rating is on an E-Flex drive?

Issue:
E-Flex voltage rating
 
Product Line:
Class 8839
 
Environment:
All Types
 
Cause:
None
 
Resolution:
The type number on the label indicates the voltage rating.  Example if the Type number is EFDJG4VY the "4" indicate 460v.  A "2" would indicate 230v. 
 
Was this helpful?
What can we do to improve the information ?