Technical FAQs

Ask a Question

Is there a motor rating for 208V applications with the GV7 manual motor starters?

Issue:
Is there a motor rating for 208V applications with the GV7 manual motor starters?

Product Line:
IEC Manual motor starters/protectors - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
These starters do not have 200V/208V ratings - The 230V ratings are the lowest voltage available.
 
Was this helpful?
What can we do to improve the information ?