Technical FAQs

Ask a Question

Will the VW3A1101 keypad come with the ATV61 or ATV71 standard drive when you order it?

Issue:
Will the VW3A1101 keypad come with the ATV61 or ATV71 standard drive when you order it?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Wants to know if the graphics keypad will come with the drive when you order it.

Resolution:
Yes the keypad comes with the ATV61 or ATV71 drive when you order the drive.   If you add the suffix letter Z it will delete the keypad when ordering the drive.
Was this helpful?
What can we do to improve the information ?