Technical FAQs

Ask a Question

Will the ATV61 and ATV71 drives have a built in +24vdc power supply?

Issue:
Will the ATV61 and ATV71 drives have a built in +24vdc power supply?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Wants to know if the ATV61 or ATV71 drive comes with its own +24vdc supply for the logic inputs

Resolution:
yes, the ATV61 and ATV71 drives both have internal 24vdc power supplies.  This power supply is designed to be used for the turning on the drives logic inputs when the drive is set up for sink mode.
Was this helpful?
What can we do to improve the information ?