Technical FAQs

Ask a Question

What is the option to get an 5% line reactor on the enclosed E-Flex drives?

Issue:
What is the option to get an 5% line reactor on the enclosed E-Flex drives?

Product Line:
E-Flex 61

Environment:
All with Mod A09

Cause:
Needs to order the E-flex Drive with a 5% line reactor.

Resolution:
Modification A09 will replace the standard DC choke with the optional 5% line reactor.
Was this helpful?
What can we do to improve the information ?