Technical FAQs

Ask a Question

Does Schneider Electric Solar offer a 10kW 3-PH grid-interactive inverter for wind generators?

Since the Bergey Gridtek10 was discontinued, we no longer offer a strictly grid tie wind inverter, 
however it is possible to use XW+NA in a 3-PH configuration (requires 3 inverters and a battery bank), 
supplying the battery directly with rectified (pulsed DC) from a 3-PH wind generator and incorporate diversion 
controllers between the battery and dump loads. The would require (6) C40 diversion controllers each 
with a dedicated dump load (48VDC water heating elements). 
Was this helpful?
What can we do to improve the information ?