Technical FAQs

Ask a Question

Is the J250R IEC Rated per IEC 60529?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Cause:
Standards clarification

Resolution:
Yes, the J250R meets IEC 60529 standards for Ingress Protection Code IP43. 
Was this helpful?
What can we do to improve the information ?