Technical FAQs

Ask a Question

What do the LED's indicate on the ATV58 devicenet card?

Issue:
LED indicators
 
Product Line:
ATV58
 
Environment:
All models and serial numbers with VW3A58309U option card.
 
Cause:
None
 
Resolution:
DIAGNOSTICS
Visually inspect the combined Module/Network Status (MNS) LED indicator at power-up to ensure that the following sequence occurs:
1. The LED glows red for 1 second upon application of power.
2. The LED glows green for approximately 0.25 seconds.
3. The LED glows red for approximately 0.25 seconds.
4. The LED glows green.

LED status indication.

Off
Device is not on-line
• The device has not completed the Dup_MAC_ID test yet.
• The device is not powered.

Green
Device is operational, online, and connected
The device is operating in a normal condition. It is allocated to a master.

Flashing Green
1. Device is operational and on-line, but not connected
2. Device is on-line but needs commissioning  
The device is on-line and operating in a normal condition, but network connections are not established.
    • The device has passed the Dup_MAC_ID test and is on-line, but has not established connections to other nodes.
    • The device is not allocated to a master.
    • Configuration is missing, incomplete, or incorrect. 

Flashing Red
Minor fault and/or connection time-out
• The device has experienced a recoverable fault.
• One or more I/O connections timed out.

Red
Critical fault or critical link failure
The card has an unrecoverable fault and may need replacing.
The device has detected an error that has rendered it incapable of
communicating on the network (duplicate MAC ID or bus turned off).

Flashing Red and Green
Communication fault
The device has detected a Network Access error and is in the
Communication Faulted state. The device has subsequently received
and accepted an Identify Communication Faulted Request—Long
Protocol message.

Flash rate:
  1.  The flash rate of the LED is approximately 1 flash per second. The LED is on for about 500 ms and off for about 500 ms.
  2.  The LED glows red for 250 ms, then glows green for 250 ms. 
Was this helpful?
What can we do to improve the information ?