Technical FAQs

Ask a Question

How do you convert an HOA to HOC on an enclosed E-Flex, M-Flex or MCC drive?

Issue:
How  do you convert an HOA to HOC on an enclosed E-Flex, M-Flex or MCC drive?

Product Line:
E-Flex, M-Flex or MCC

Environment:
All enclosed ordered with an HOA switch

Cause:
Enclosed drive was ordered with an HOA and they need to change the controls for auto to be network control.

Resolution:
Change the auto settings in the program from analog input and terminal CMD to com card.
example
if CMD channel 2 is terminal change it to Com card
If REf 1 B channel is AI2 change it to Com card.
 
Was this helpful?
What can we do to improve the information ?