Technical FAQs

Ask a Question

What can cause a state of NST on an ATS48 Soft Start?

Issue:
The state is nSt
 
Product Line:
ATS48
 
Environment:
All models and serial numbers
 
Cause:
Forced to freewheel stop by a logic input or the serial link.

Resolution:
The nSt state is not a fault condition but is one that can be forced via a logic input or through the network via serial link.
 
Was this helpful?
What can we do to improve the information ?