Technical FAQs

Ask a Question

Will the ATV61 and ATV71 come standard with modbus?

Issue:
Will the ATV61 and ATV71 come standard with modbus?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to know if the drive comes with integrated modbus.

Resolution:
Yes
The ATV61/71 drive will come with an integrated RJ45 connection for modbus or CANopen.
 
Was this helpful?
What can we do to improve the information ?