Technical FAQs

Ask a Question

Is the S-flex system available with forward and reverse motor control?

Issue:
Is the S-flex system available with forward and reverse motor control?
 
Product Line:
SFD21 and SFD212, all enclosed S-flex systems.
 
Environment:
All models, All serial numbers
 
Cause:
Customer needs to be able to run their motor forward and reverse in an S-flex system.
 
Resolution:
The standard S-Flex wiring uses the F and R terminals for Run Forward and Run Permissive. 

The RES terminal is typically unused and may be assigned and wired to operate the drive in Reverse.  Assign parameter F113 to 3 (Reverse). 




 
Was this helpful?
What can we do to improve the information ?