Technical FAQs

Ask a Question

Do we offer a NEMA 4X protection tube for the XUSL4E30H121N light curtain, for food environment?

Issue:
Do we offer a NEMA 4X protection tube for the XUSL4E30H121N light curtain, for food environment?

Environment:
Light Curtain,  XUSL, IP69K

Cause:
Need NEMA 4X or greater protection tube for XUSL4E30H121N light curtain being used in a food environment.

Resolution:
We do not offer a tube for the XUSL4E30H121N. The XUSL4E30H121N is 1210mm tall, the tallest tube offered is only 1260mm.  They may consider the XUSL4E30H106N with the XUSL4E30H106LWC protection tube. The XUSL light curtains are IP69K rated.
Was this helpful?
What can we do to improve the information ?