Technical FAQs

Ask a Question

Where can I find the heat dissipation of the enclosed M-FLEX units?

Where can I find the heat dissipation of the enclosed M-FLEX units?
Issue: 
Where can I find the heat dissipation of the enclosed M-Flex units?
 
Product Line:
Enclosed M-Flex Altivar 61 and Altivar 71
 
Environment:
All serial numbers
 
Cause:
N/A
 
Resolution:
For the heat dissipation see the attached document from the enclosed M-FLEX manual, document number 30072-451-52
              
Was this helpful?
What can we do to improve the information ?