Technical FAQs

Ask a Question

Does an ATV212W drive require a conduit kit?

Issue:
Does an ATV212W drive require a conduit kit?

Product Line:
ALTIVAR 212 ATV212

Environment:
ATV212W models

Cause:
Is a conduit kit required to achieve the Nema 12 rating?

Resolution:
No.  The ATV212W drive has IP54/Type 12 enclosure rating.  Knockouts are provided for conduit landing.
Was this helpful?
What can we do to improve the information ?