Technical FAQs

Ask a Question

Do we have a recommended 9 pin sub D connector when replacing the Metsys N2 VW3A3313 card to a VW3A3318 option card?

Issue:
Do we have a recommended 9 pin sub D connector when replacing the Metsys N2 VW3A3313 card  to a VW3A3318 option card?

Product Line:
Altivar ATV61 with a VW3A3313 or VW3A3318 option card.

Environment:
All

Cause:
They ordered the new VW3A3318 card with the screw terminals but they have a male sub D connector that they want to connect to the drive.

Resolution:
We do not have a recommended sub D connector.  You will have to go to a 3rd party company like Phoenix connectors to see if they have a recommended part.

see page 14 of the attached VW3A3318 manual for recommended wiring.
Was this helpful?
What can we do to improve the information ?