Technical FAQs

Ask a Question

What is the form G50XX for combination starters? (eg G505)

Issue:
What is the form G50XX for (eg G505)

Product Line:
8538 Combination NEMA Starters - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
The Form G50XX is for wired/unwired terminal blocks installed at the factory.  In the past any number could be specified, but now they must be ordered in groups of five (eg G505, G5010, etc).  Whether they are wired or unwired would have been specified at the time of order and cannot be determined from the form code alone.

 
Was this helpful?
What can we do to improve the information ?