Technical FAQs

Ask a Question

What is the max current rating on the ATV61 and ATV71 drives 10vdc power supply?

Issue:
What is the max current rating on the ATV61 and ATV71 drives 10vdc power supply?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to connect some small LEDs using the 10vdc supply so they need to know the max current current ratings.

Resolution:
The max current rating  is 10mA max @ 10vdc.
 
Was this helpful?
What can we do to improve the information ?