Technical FAQs

Ask a Question

On the Altivar ATV630 process drive what does it mean by embedded control (PLC, RTU, HMI)?

Issue:
On the Altivar ATV630 process drive what does it mean by embedded control (PLC, RTU, HMI)?

Product Line:
Altivar ATV630 process drive

Environment:
All

Cause:
PLC control? Does the drive have a built in PLC?

Resolution:
Embedded control by PLC means the process drive has a built in Ethernet TCPIP card that can be controlled over a PLC controller.
RTU control means modbus control
HMI control means keypad or local control.

 
Was this helpful?
What can we do to improve the information ?