Technical FAQs

Ask a Question

What is the IP rating of the VW3A1006 keypad?

Issue:
What is the IP rating of the VW3A1006 keypad?

Product Line:
ALTIVAR 12, ALTIVAR 312

Environment:
All

Cause:
What is the IP rating of the VW3A1006 keypad?

Resolution:
This keypad is rated for IP54.
Was this helpful?
What can we do to improve the information ?