Technical FAQs

Ask a Question

How does the XW AGS know when the generator is running?

All firmware revisions 2.3 and higher use the presence of AC voltage at the AC2 input to determine if the generator is running EXCEPT Type14, 
which does not monitor a run signal at all. This feature was implemented in Type14 for extremely cold environments where it may take several crank tries 
to start the generator, resulting in fault related to too many start tries (F200).
Was this helpful?
What can we do to improve the information ?