Technical FAQs

Ask a Question

What is the replacement coils for Panelboard 8903PB Lighting Contactors?

Issue:
What is the replacement coils for Panelboard 8903PB Lighting Contactors?

Product Line:
8903PB Panelboard Lighting Contactors - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
The replacement coils are as follows:
9998PBV02 - 120 Vac
9998PBV08 - 208 Vac
9998PBV39 - 240/277 Vac
9998PBV28 - 480 Vac
Dual voltage coils are no longer available
 
Was this helpful?
What can we do to improve the information ?