Technical FAQs

Ask a Question

Does the ATV32 series drive support Fast Device Replacement (FDR) function for Ethernet IP?

Issue:
Does the ATV32 series drive support Fast Device Replacement (FDR) function for Ethernet IP?
 
Product Line:
ATV32 series drives
 
Environment:

All models, All serial number
 
Cause:

Information unavailable in current literature.
 
Resolution:
No, The Fast Device Replacement function of the ATV32 series drive is only available for Modbus TCP protocol.  It is not available for Ethernet IP.
Was this helpful?
What can we do to improve the information ?